AXIS#.TUNING.TARGETBANDWIDTH
Description
AXIS#.TUNING.TARGETBANDWIDTH displays the target bandwidth calculated by the most recent QuickTune procedure since the drive booted up.
-
If AXIS#.TUNING.USERBANDWIDTH is set to 0, AXIS#.TUNING.BANDWIDTH will be set to the most recently calculated AXIS#.TUNING.TARGETBANDWIDTH at the end of QuickTune procedure.
This value is updated with every QuickTune procedure regardless of AXIS#.TUNING.USERBANDWIDTH. If the target bandwidth cannot be calculated, AXIS#.TUNING.TARGETBANDWIDTH will be set to 0.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-12-02-000 |
- |
General Information
| Type | Read Only |
| Units | Hz |
| Range | N/A |
| Default Value | N/A |
| Data Type | Double |
| See Also | AXIS#.TUNING.QUICKTUNE.START |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.TUNING.TARGETBANDWIDTH |
5021h |
07h |
Signed32 |
- |
1000:1 |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5041 |
1 |
5041 (0x13b1) |
AXIS1.TUNING.TARGETBANDWIDTH |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.TUNING.TARGETBANDWIDTH |
5041 |
Float |
Read Only |
- |